TI Offers Single Device, Optical Power Meter Functionality with the OPT3002 Light-to-Digital Sensor, Now at Mouser
August 30, 2016 - Mouser Electronics, Inc. is now stocking the OPT3002 light-to-digital sensor from Texas Instruments (TI). Greatly improving system performance over standard photodiodes and photoresistors, the fully-integrated OPT3002 delivers the functionality of an optical power meter all within a single small device. Offering a wide spectral bandwidth, flexible and automated light measuring over a 23-bit effective dynamic range, and a simplified software and set-up configuration, this low-power optical sensor is ideal for use in optical spectral systems that require detection of a variety of wavelengths, such as optically-based diagnostic systems, or even as a low-power, battery-operated wake-up sensor.
The Texas Instruments OPT3002 light-to-digital sensor, available from Mouser Electronics, is an ambient light sensor (ALS) with a digital output integrated circuit. The OPT3002 features a wide spectral bandwidth that measures light within the device spectral range of 300 nm to 1,000 nm. Using the device's built-in, full-scale setting feature, the OPT3002 can take light measurements from 1.2nW/cm2 up to 10mW/cm2 without the need to manually select the full-scale ranges. This built-in functionality enables capturing of light measurements over a 23-bit effective dynamic range, with results compensated for dark-current effects and other temperature variations.
The OPT3002 captures measurements in either a continuous or single-shot fashion. The optical sensor measures the ambient light and reports the optical power readings directly from its two-wire, I2C- and SMBus-compatible serial interface. The interrupt pin system can also summarize measurement results with one digital pin. With fully-operational power consumption as low as 0.8 μW at 0.8 SPS on a 1.8V supply, the OPT3002 Light-to-Digital Sensor can be incorporated into a broad array of low-power, sensor-based applications, including security detection systems, system wake-up circuits, medical and scientific instrumentation, lighting controls, tablet and notebook computers and home automation.
Texas Instruments' OPT3002 light-to-digital sensor is available in a compact, 6-USON package that measures only 2.0 mm × 2.0 mm × 0.65 mm. To evaluate the OPT3002 under various conditions, the device is also supported by the OPT3002EVM ambient light sensor evaluation module. The OPT3002EVM features a small form factor module based on two PCBs (a data acquisition board and test board), includes intuitive GUI software, and is designed with 100mil-spaced test points for easy experimentation with external controllers.
To learn more about TI's OPT3002 light-to-digital sensor and evaluation module, visit http://www.mouser.com/new/Texas-Instruments/ti-opt3002-sensor/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 600 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com