Mouser Now Stocking Microchip's MCP9600, Industry's First Integrated Thermocouple EMF-to-Temperature Converter
November 30, 2015 - Mouser Electronics, Inc. is now stocking the MCP9600 thermocouple EMF to temperature converter from Microchip Technology. The MCP9600 is the first thermocouple-conditioning integrated circuit to combine precision instrumentation, a precision temperature sensor and a precision, high-resolution analog-to-digital converter (ADC), in addition to a math engine preprogrammed with the firmware to support a broad range of standard thermocouple types. The MCP9600 simplifies thermocouple designs by integrating these discrete devices into one chip, reducing board area, cost, and power consumption.
The MCP9600 thermocouple EMF to temperature converter, now available from Mouser Electronics, converts thermocouple electromotive force (EMF) to degrees Celsius with integrated cold-junction compensation to avoid incorrect measurements. It corrects the thermocouple nonlinear error characteristics of eight thermocouple types (K, J, T, N, S, E, B, R) and outputs temperature data accurate to ±1.5 degrees Celsius for the selected thermocouple. The MCP9600 provides designers with the first plug-and-play solution for creating thermocouple-based designs, because it eliminates the design expertise required for a discrete implementation, such as firmware development using a microcontroller's math engine.
The MCP9600 includes user-programmable registers, which provide design flexibility for various temperature-sensing applications, including low-power modes for battery-powered applications, adjustable digital filter for fast transient temperatures, and four individually programmable temperature alert outputs that can be used to detect multiple temperature zones. The temperature alert limits have multiple programmable configurations such as alert polarity as either an active-low or active-high push-pull output, and output function as comparator mode (useful for thermostat-type operation) or interrupt mode for microprocessor-based systems. In addition, the alerts can detect either a rising or a falling temperature with up to 255 degrees Celsius hysteresis.
This sensor uses an industry-standard 2-wire, I2C-compatible serial interface and supports up to eight devices per bus by setting the device address using the ADDR pin. The MCP9600 supports thermal management and measurement applications in harsh environments, including those in the industrial, consumer, automotive, aerospace, and petrochemical markets.
To learn more, visit http://www.mouser.com/new/microchip/microchip-mcp9600-converter/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Microchip Technology
Microchip Technology Inc. is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality.
Microchip Technology Inc. has acquired Micrel. For more information, visit http://www.mouser.com/microchip/.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President, Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com