Lumileds Latest LUXEON CoB Core Range LEDs, Now at Mouser, Offer High Density in a Small Surface
April 5, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking LUXEON CoB Core Range (Gen 4) LEDs from Lumileds. These LEDs offer high flux densities in a small light emitting surface (LES), enabling double the luminous flux of the third generation of LUXEON CoB Core Range devices. The high-density CoBs can achieve the highest center beam candlepower (CBCP) in narrow-beam (less than 20-degree) spotlight applications.
The fourth generation of Lumileds LUXEON CoB Core Range LEDs, available from Mouser Electronics, feature a single optical LES of 13, 15, or 19 mm that provides high flux densities and high efficacy. LUXEON CoB Core Range (Gen 4) LED arrays are offered over a color temperature of 3000K to 4000K and CRI of 80 or 90. The CoBs provide the industry's lowest thermal resistance, enabling smaller heat sinks and optics for lower overall system cost. The MCPCB substrate is also more robust than ceramic substrates that are subject to cracking upon assembly or use.
All the LUXEON CoB Core Range LED devices are binned with a single 3-step (80 and 90 color index rating) MacAdam ellipse to ensure optical performance in retrofit lamps and spotlight applications. LUXEON CoB Core Range LEDs are all hot-tested at 85 degrees Celsius, so that luminaire design is simplified and testing can be minimized.
The LUXEON CoB Core Range LEDs from Lumileds are designed for a broad array of general purpose and directional lighting applications including architectural lighting, downlights, high bay and low bay fixtures, and spotlights.
To learn more, visit www.mouser.com/lumileds-luxeon-cob-leds.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 22 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Lumileds
Lumileds is the global leader in light engine technology. The company develops, manufactures and distributes groundbreaking LEDs and automotive lighting products that shatter the status quo and help customers gain and maintain a competitive edge. With a rich history of industry "firsts," Lumileds is uniquely positioned to deliver lighting advancements well into the future by maintaining an unwavering focus on quality, innovation and reliability.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com