Mouser Now Stocking the Atmel ATtiny104 Xplained Nano Evaluation Kit for the ATtiny102/104 AVR Microcontrollers
April 5, 2016 - Mouser Electronics, Inc. is now stocking the ATtiny104 Xplained Nano from Atmel. Designed as an evaluation kit for Atmel's recently launched ATtiny102 and ATtiny104 8-bit AVR® microcontrollers, the ATtiny104 Xplained Nano board enables designers to gain access to all the key features of the Atmel ATtiny microcontrollers without the need for external programming tools.
The Atmel ATtiny104 Xplained Nano, available from Mouser Electronics, was developed specifically to accelerate the design process and support Atmel's 8-bit ATtiny102 and ATtiny104 AVR microcontrollers. Part of Atmel's new AVR Tiny portfolio, these devices can run up to 12MIPS at 12 MHz, and feature 1 kByte of flash, 32 bytes of SRAM, and a Universal Synchronous/Asynchronous Receiver/Transmitter (USART). The ATtiny104 Xplained Nano board offers a user button and LED, as well as access to all of the input and output (I/O) pins and other features of the microcontroller for easy evaluation. In addition, the board has an Atmel Mini Embedded Debugger (mEBDG), which is essentially a composite USB device of two interfaces: a debugger and a Virtual COM Port. The mEBDG features an auto-ID for board identification in Atmel Studio, one green board status LED, and programming capabilities.
Using the ATtiny 104 USART interface, the Xplained Nano board can also communicate with a serial terminal over USB for debugging and verification, and can stay connected to the terminal program even during chip re-programming. The onboard programmer can be completely disconnected from the host microcontroller or it can be used to program any other microcontroller with the Atmel Tiny Programming Interface (TPI).
The ATtiny104 Xplained Nano is supported by Atmel's development ecosystem, including Atmel Studio 7, an integrated development environment (IDE) that gives designers a seamless and easy-to-use environment for coding, building, simulating, programming, and debugging applications for Atmel microcontrollers. The ATtiny104 Xplained Nano operates at a supply voltage of 5V and is ideal for prototyping a variety of small applications including logic replacement and cost-optimized applications in the consumer, industrial and home automation markets.
To learn more, visit http://www.mouser.com/new/atmel/atmel-attiny104-nano/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Atmel
Atmel Corporation is a global leader in designing, manufacturing and marketing advanced semiconductors including microcontroller (MCU), programmable logic, and nonvolatile memory. By combining these core technologies, Atmel meets the evolving and growing needs of today's electronic system design engineer through the production of general purpose and application specific system level integrated chips. Atmel's world class expertise and wealth of experience in system-level integration enable all of Atmel's products to be developed from their constituent blocks with minimum delay and risk.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President, Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com