Texas Instruments' TPS1685 Stackable Integrated Hotswap eFuses, Now at Mouser, Provide Maximum Protection for Modern Data Centers

New Product Announcement

Connect With Us


Learn more about the TPS1685 stackable integrated hotswap eFuses
Learn more about the TPS1685 stackable integrated hotswap eFuses

September 24, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the TPS1685 stackable integrated hotswap eFuses from Texas Instruments. The TPS1685 is the industry's first 48V integrated hot-swap eFuse with power-path protection to support the needs of modern data centers, enabling designers to reach power levels beyond 6kW. The TPS1685 is a compact and reliable solution for server and high-performance computing, graphics, and hardware accelerator cards, data center switches and routers, and fire alarm control panels.

The Texas Instruments TPS1685 hotswap eFuses, now available at Mouser, feature a fast and accurate sense analog current monitor that facilitates predictive maintenance and advanced dynamic platform power management. The TPS1685 eFuses operate at a 9V to 80V input voltage range and provide robust defense against overloads, short-circuits, and excessive inrush current.

The TPS1685 eFuses also offer an active high enable input with adjustable undervoltage lockout (UVLO) and adjustable overvoltage protection. Integrating functionalities typically provided by external sense resistors and current-sense amplifiers, the TPS1685 eFuses simplify designs and reduce solution sizes by up to 50%. The TPS1685 eFuses feature an operating temperature range of -40°C to +125°C, and the 6 x 5 mm2 QFN package has IPC9592B clearance for 60V.

To learn more, visit https://www.mouser.com/new/texas-instruments/ti-tps1685-efuses/

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764