When Will 5G Enter Industrial TSN?
Image Source:
Tierney/Shutterstock.com
By Jeff Shepard for Mouser Electronics
Published March 7, 2022
Time-sensitive networking (TSN) is being deployed across a growing number of applications. But for 5G-based
wireless TSN (WTSN), it’s still early. WTSN will open new applications, such as mobile robots, electric
power grids, chemical plants, smart cities, and other geographically dispersed applications, plus automotive and
transportation systems that can’t be connected to wired TSN networks (Figure 1). WTSN
will bring revolutionary new capabilities to TSN. It will also increase the deployment flexibility and reduce
the installation costs of TSN. 5G-based WTSN is tantalizingly close, but it’s not quite ready for
deployment; the needed standards are still evolving and emerging, and the hardware and software are under
development.
Figure 1: 5G-WTSN will expand the use of time-sensitive networking to new
applications not possible with wired TSN implementations. (Source: wladimir1804/Stock.Adobe.com)
Many industrial applications require fast, deterministic communication for real-time control. In IEEE 802,
definitions have been added to make Ethernet deterministic. 3GPP Release 16 adds support for integration of TSN
protocols to guarantee latencies in 5G communications. The pending Release 17 will take 5G further toward
supporting WTSN. The upcoming IEC/IEEE 60802 profile specifies the application of TSN for industrial automation
and gives guidelines regarding the TSN support needed from 5G.
In addition to the 3GPP, IEC, and IEEE, several efforts are underway to integrate 5G with TSN to create combined
WTSN/TSN industrial networks. The EU-funded 5G-SMART is a consortium of industry partners and research
institutes exploring 5G-enabled smart manufacturing concepts, including WTSN. The 5G Alliance for Connected
Industries and Automation (5G-ACIA), has identified how 5G has all the essential capabilities required to
interwork with TSN for industrial automation.
Four main areas are included in IEEE 802.1 TSN standards: Time synchronization, bounded latency, reliability, and
resource or network management. This article looks at how each of those four areas maps into 5G and explores how
5G will move WTSN forward to the next generation of industrial automation devices and the industrial internet of
things (IIoT). It reviews existing and emerging standards in Release 16, Release 17, and IEC/IEEE 60802, looking
at how 5G ultra-reliable low latency communication (URLLC) will be enhanced with direct device-to-device
communication enabled by sidelink, which doesn’t require relaying data through the network for
communication to take place. It also considers radio spectrum options and deployment choices such as
architectures for hybrid public/private networks and network slicing.
5G Time Synchronization
The move to basic 5G services didn’t result in any fundamental change in radio network time synchronization
needs, but WTSN will require more stringent local synchronization accuracy for 5G nodes. The telecom industry
has standardized the IEEE 1588 precision time protocol (PTP) to support synchronization requirements in the
millisecond range. The 3GPP TS 23.501 specification addresses the integration of a 5G network into a TSN
synchronization network and supports WTSN. IEEE 1588 includes the development of application-specific profiles.
One result is the IEEE 802.1AS general PTP (gPTP) profile within the TSN standards and implementations defined
in the TSN profile for industrial automation.
Industrial automation networks benefit from fast initialization and time synchronization in a few seconds.
It’s also desirable to use off-the-shelf network interconnect cards with lower cost and less accurate
oscillators. Compared with the physical syntonization (frequency alignment) technique used in other PTP
implementations, gPTP uses a logical syntonization technique together with real-time measurements of path and
device delays to achieve fast and accurate time alignments.
The exchange of time-stamped messages is used to communicate time from a master clock to the various bridge and
end-point devices. Unlike other PTP implementations, gPTP also uses time-stamped messages to calculate frequency
offsets and adjusts for these during operation.
5G Bounded Latency
URLLC and sidelink are key features in Release 17 that support bounded (ultra-low and deterministic) latency in
WTSNs. URLLC is designed to ensure data delivery within specific latency bounds from tens of milliseconds to 1
millisecond and desired reliability levels from 99% to 99.999%, as defined by application requirements.
As noted above, sidelink is a new communication paradigm enabling 5G devices to communicate directly without
relaying their data via the network. In conventional uplinks and downlinks, the network centrally controls
resources and link adaptations. In sidelinks, each device performs both functions locally, gaining more control
of how to use network resources. The upcoming Release 17 is expected to add support for sidelink-based relaying
and possibly even multi-link relaying. As sidelink capabilities expand, the combination of sidelink and URLLC
will increasingly support the use of 5G-based WTSN in the IIoT (Figure 2).
Figure 2: Sidelink enables network devices to communicate directly without
relaying their data via the network and is expected to expand WTSN 5G deeper into the IIoT. (Source:
metamorworks/Stock.Adobe.com)
Sidelink supports expanded use cases for 5G. For example, restricting the communication link to one hop in
mission-critical industrial applications greatly reduces latency. Public safety networks could also benefit from
sidelink’s ability to provide direct communication between devices. In applications where milliseconds
matter, sidelink is expected to be a significant development given the capacity and latency improvements
associated with the move from two-hop communication through a 5G base station to one-hop, device-to-device
connections.
Future iterations of sidelink multi-hop relaying are expected to support lower power consumption when used in an
IIoT network. Another potential use case is multi-hop relaying, where multiple sidelink connections are used to
leap from device to device, overcoming link budget constraints and eventually even replacing some of the
Bluetooth and Wi-Fi links that currently connect IIoT devices.
WTSN In Converged Networks
The anticipated IEC/IEEE 60802 standard will provide a basis for interoperability in industrial automation
converged networks. These converged networks will include industrial Ethernet and wireless, including 5G and/or
Wi-Fi communications. IEC/IEEE 60802 is a joint effort between IEC SC65C/MT9 and IEEE 802, with the first
official release expected in 2022. The standard will include details for the application of TSN in industrial
automation, including guidelines for integrating 5G-based WTSN. Once released, all the components for building a
TSN/WTSN network will be standardized using IEC/IEEE 60802.
Two device types, bridges and end stations, are included in IEC/IEEE 60802. Initially, the standard will include
two classes of devices for both device types. Feature-rich devices will be called Class A. Class B devices will
support a smaller set of features. Devices belonging to the same class will have the same mandatory and optional
TSN/WTSN capabilities.
All device types and classes require the Link Layer Discovery Protocol (LLDP) (802.1AB) and time synchronization.
LLDP supports the discovery of the network topology and neighbor information. In the case of time
synchronization, Class A devices are expected to support a minimum of three-time domains, and Class B devices
will support at least two-time domains. Class A devices will be required to support a range of TSN functions
(including Scheduled Traffic, Frame Preemption, Per-Stream Filtering and Policing, Frame Replication and
Elimination for Reliability (FRER), and TSN configuration), but that will be optional for Class B devices.
The ultimate goal of IEC/IEEE 60802 is to provide a sufficiently structured TSN/WTSN profile for industrial
automation that is also flexible and offers a wide range of options to support the deployment of convergent
networks that efficiently blend different protocols into a single network.
Private 5G Networks for WTSN
Converged deployments may find their first implementations on private 5G networks, also called non-public
networks (NPNs). In addition to supporting converged networks, 5G is offering a unified architecture that
supports the needs of various industrial applications, including three primary categories of service: Massive
machine type communication (mMTC) with connection density of up to 100 nodes per square meter, enhanced mobile
broadband (eMBB) with peak data rate of up to 10Gbps, and URLLC, providing as little as one-millisecond latency
with > 99.999% reliability. With these various choices, users can optimize the quality-of-service (QoS) for
specific applications. Unlike other wireless technologies such as 4G or Wi-Fi, 5G provides guaranteed QoS for
critical industrial applications.
Deployment of 5G NPNs is not limited to the licensed spectrum bands; it can take advantage of unlicensed spectrum
such as the 2.4GHz, 5GHz, and 6GHz bands already used by Wi-Fi, Bluetooth, ZigBee, and other protocols.
Unlicensed spectrum is implicitly open for shared use and has already been included in some 4G-LTE networks. 5G
in unlicensed spectrum can be implemented in two ways.
Standalone unlicensed NPNs operate entirely in the unlicensed spectrum. Unlicensed operation of 5G is expected to
be led by private organizations that do not offer public mobile networking services and are focused on
non-critical use cases. One of its main attractions is that it can be deployed with no need for expensive
licensed spectrum. The Multefire protocol is the corresponding 4G implementation on unlicensed spectrum. It uses
a listen-before-talk (LBT) protocol to co-exist with other spectrum users in the same band efficiently. Without
sidelink, ultra-low latency may not be possible in standalone unlicensed 5G deployments.
NPNs using a combination of licensed and unlicensed spectrum are called licensed anchor operations. The
corresponding capability in LTE is licensed-assisted access (LAA), where the unlicensed band is used to
supplement the available licensed band. Licensed anchor operation is expected to be used by operator-deployed
private networks that need extra capacity.
5G Network Slicing
Network slicing is another tool network engineers have for getting the maximum benefit from 5G in focused
industrial applications. The concept of network slicing is new with 5G and enables the creation of multiple
logical networks over a single physical infrastructure. Each of the logical networks can be tailored to the
specific requirements of an application (Figure 3). Various functions such as business
processes, logistics operations, and time-critical processes and manufacturing can be operated on dedicated,
isolated networks. Creating networks within a network is expected to be especially useful in converged networks
and NPNs.
Figure 3: Network slicing can create multiple logical networks over a common
physical infrastructure, with each logical network optimized for specific application requirements. (Source:
metamorworks/Stock.Adobe.com)
Network slicing can be a powerful tool for resource and network management. For example, a public 5G network can
be sliced to include a private 5G network isolated and dedicated to specific activities. 5G NPNs can serve a
range of heterogeneous industrial communication requirements with different QoS demands. Some slices can be
dedicated to non-time-sensitive communications, while other slices can support moderate QoS levels required for
closed-loop-control of industrial processes, and dedicated slices can be created to provide the higher QoS
required for real-time communications with mobile robots.
Management of computing, storage, and general networking resources can be improved using network slicing to
maximize the efficiency of resource utilization across an organization. It also enables the development of
slice-specific policies for security, privacy, access levels, and more.
Summary
5G-based WTSN will bring revolutionary new capabilities to TSN, but it’s not ready for deployment. Once it
arrives, capabilities such as time synchronization, bounded latency, sidelink, and interoperability across
various device classes will help speed the deployment of 5G-based WTSNs. Support for converged networks, private
networks, and network slicing will provide improved resource allocation and network management. And 5G-based
WTSN will increase the deployment flexibility and reduce the installation costs in existing TSN installations.
Author Bio
Jeff was a
co-founder of Jeta Power Systems, a maker of high-wattage switching power supplies acquired by Computer
Products. Jeff is also an inventor. His name is on 17 U.S. patents in the fields of thermal energy harvesting
and optical metamaterials. He is an industry source and frequent speaker on global trends in power electronics.
He has been invited to speak at numerous industry events, including the Plenary Session of the IEEE Applied
Power Electronics Conference, Semicon West, Global Semiconductor Alliance Emerging Opportunities Conference, IBM
Power and Cooling Symposium, and Delta Electronics Senior Staff Seminar on Global Telecommunications Power. Jeff
has a Master's degree in Quantitative Methods and Mathematics from the University of California, Davis. Jeff has
been writing about power electronics, electronic components, and other technology topics for over 30 years. He
started writing about power electronics as a senior editor at EETimes. He founded Powertechniques, a power
electronics design magazine with a monthly circulation of over 30,000. He subsequently founded Darnell Group, a
global power electronics research and publishing firm. Among its activities, Darnell Group published
PowerPulse.net, which provided daily news for the global power electronics engineering community. He is the
author of a switch-mode power supply textbook, titled "Power Supplies," published by the Reston division of
Prentice Hall.